public interface FieldExpression extends Field
Field
) which has exactly one dependent
variable (see FieldVariable
), where the field function defintions
is implemented using the NX Expression sub-system Expression
. DisplayableObject.ObjectFont, DisplayableObject.ObjectWidth
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat
Modifier and Type | Method and Description |
---|---|
void |
editFieldExpression(String fieldExpString,
Unit unitType,
FieldVariable[] indepVarArray,
boolean updateFlag)
Edit the expression field.
|
copyAsTableToPart, copyToPart, createCopyInPart, createTableInPart, delete, getDependentVariables, getDescription, getFieldEvaluator, getIdLabel, getIndependentVariables, getSpatialMap, isLocked, isUserField, rename, setDescription, setIdLabel, setSpatialMap, xygraph, xygraph, xygraph, xygraphAndReturnPlots, xygraphScaleAndReturnPlots
blank, color, highlight, isBlanked, layer, lineFont, lineWidth, nameLocation, redisplayObject, removeViewDependency, setColor, setLayer, setLineFont, setLineWidth, setNameLocation, unblank, unhighlight
deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
void editFieldExpression(String fieldExpString, Unit unitType, FieldVariable[] indepVarArray, boolean updateFlag) throws NXException, RemoteException
FieldFormula
.
fieldExpString
- expression string to be associated with the field unitType
- unit of the fieldindepVarArray
- independent variables to be associated with the fieldupdateFlag
- update flagNXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.