Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static MirrorCertificationBuilder.EyeMethodType |
MirrorCertificationBuilder.EyeMethodType.MAXIMUM_DISTANCE
Represents using the maximum distance
|
static MirrorCertificationBuilder.EyeMethodType |
MirrorCertificationBuilder.EyeMethodType.MEAN_DISTANCE
Represents using the mean distance
|
static MirrorCertificationBuilder.EyeMethodType |
MirrorCertificationBuilder.EyeMethodType.MINIMUM_DISTANCE
Represents using the minimum distance
|
Modifier and Type | Method and Description |
---|---|
MirrorCertificationBuilder.EyeMethodType |
MirrorCertificationBuilder.eyeMethod()
Returns the method to calculate the eye location based on the distance from the eyellipse to the mirror pivot.
|
static MirrorCertificationBuilder.EyeMethodType |
MirrorCertificationBuilder.EyeMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.EyeMethodType |
MirrorCertificationBuilder.EyeMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.EyeMethodType[] |
MirrorCertificationBuilder.EyeMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorCertificationBuilder.setEyeMethod(MirrorCertificationBuilder.EyeMethodType eyeMethod)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.