public static class MirrorCertificationBuilder.EyeMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAXIMUM_DISTANCE
Represents using the maximum distance
|
static int |
_MEAN_DISTANCE
Represents using the mean distance
|
static int |
_MINIMUM_DISTANCE
Represents using the minimum distance
|
static MirrorCertificationBuilder.EyeMethodType |
MAXIMUM_DISTANCE
Represents using the maximum distance
|
static MirrorCertificationBuilder.EyeMethodType |
MEAN_DISTANCE
Represents using the mean distance
|
static MirrorCertificationBuilder.EyeMethodType |
MINIMUM_DISTANCE
Represents using the minimum distance
|
Modifier and Type | Method and Description |
---|---|
static MirrorCertificationBuilder.EyeMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.EyeMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.EyeMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final MirrorCertificationBuilder.EyeMethodType MAXIMUM_DISTANCE
public static final MirrorCertificationBuilder.EyeMethodType MINIMUM_DISTANCE
public static final MirrorCertificationBuilder.EyeMethodType MEAN_DISTANCE
public static final int _MAXIMUM_DISTANCE
public static final int _MINIMUM_DISTANCE
public static final int _MEAN_DISTANCE
public static MirrorCertificationBuilder.EyeMethodType valueOf(int value)
public static MirrorCertificationBuilder.EyeMethodType valueOf(String name)
public static MirrorCertificationBuilder.EyeMethodType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.