public static class WheelCoveringBuilder.SurfaceSectionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADR42
The checking surface is created as ADR 42 type
|
static int |
_CIRCLE_SECTION
The checking surface is created as circle section type
|
static int |
_EXTRUDE_SECTION
The checking surface is created as extrude section type
|
static WheelCoveringBuilder.SurfaceSectionType |
ADR42
The checking surface is created as ADR 42 type
|
static WheelCoveringBuilder.SurfaceSectionType |
CIRCLE_SECTION
The checking surface is created as circle section type
|
static WheelCoveringBuilder.SurfaceSectionType |
EXTRUDE_SECTION
The checking surface is created as extrude section type
|
Modifier and Type | Method and Description |
---|---|
static WheelCoveringBuilder.SurfaceSectionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WheelCoveringBuilder.SurfaceSectionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WheelCoveringBuilder.SurfaceSectionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final WheelCoveringBuilder.SurfaceSectionType CIRCLE_SECTION
public static final WheelCoveringBuilder.SurfaceSectionType ADR42
public static final WheelCoveringBuilder.SurfaceSectionType EXTRUDE_SECTION
public static final int _CIRCLE_SECTION
public static final int _ADR42
public static final int _EXTRUDE_SECTION
public static WheelCoveringBuilder.SurfaceSectionType valueOf(int value)
public static WheelCoveringBuilder.SurfaceSectionType valueOf(String name)
public static WheelCoveringBuilder.SurfaceSectionType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.