public static class WheelCoveringBuilder.SurfacePlaneType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PERPENDICULARTO_LOADING
The checking surface is perpendicular to the active loading plane
|
static int |
_WHEEL_PLANE
The checking surface is coplanar to the ourside of the wheels
|
static WheelCoveringBuilder.SurfacePlaneType |
PERPENDICULARTO_LOADING
The checking surface is perpendicular to the active loading plane
|
static WheelCoveringBuilder.SurfacePlaneType |
WHEEL_PLANE
The checking surface is coplanar to the ourside of the wheels
|
Modifier and Type | Method and Description |
---|---|
static WheelCoveringBuilder.SurfacePlaneType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WheelCoveringBuilder.SurfacePlaneType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WheelCoveringBuilder.SurfacePlaneType[] |
values()
Returns an array that contains the values for this enum.
|
public static final WheelCoveringBuilder.SurfacePlaneType WHEEL_PLANE
public static final WheelCoveringBuilder.SurfacePlaneType PERPENDICULARTO_LOADING
public static final int _WHEEL_PLANE
public static final int _PERPENDICULARTO_LOADING
public static WheelCoveringBuilder.SurfacePlaneType valueOf(int value)
public static WheelCoveringBuilder.SurfacePlaneType valueOf(String name)
public static WheelCoveringBuilder.SurfacePlaneType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.