Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
TransFrameListItemBuilder |
TransFrameBuilder.createTransFrameListItem()
Create a list containing all required info to generate transverse frame.
|
TransFrameListItemBuilder |
TransFrameListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
TransFrameListItemBuilder[] |
TransFrameListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
TransFrameListItemBuilderList.append(TransFrameListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
TransFrameListItemBuilderList.append(TransFrameListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
TransFrameListItemBuilderList.erase(TransFrameListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
TransFrameListItemBuilderList.erase(TransFrameListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
TransFrameListItemBuilderList.findIndex(TransFrameListItemBuilder obj)
Finds the index where the input object appears.
|
void |
TransFrameListItemBuilderList.insert(int location,
TransFrameListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
TransFrameListItemBuilderList.setContents(TransFrameListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
TransFrameListItemBuilderList.swap(TransFrameListItemBuilder object1,
TransFrameListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.