Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static StiffenerSystemBuilder.EndCutTypes |
StiffenerSystemBuilder.EndCutTypes.CONNECTED |
static StiffenerSystemBuilder.EndCutTypes |
StiffenerSystemBuilder.EndCutTypes.FLANGE_FREE |
static StiffenerSystemBuilder.EndCutTypes |
StiffenerSystemBuilder.EndCutTypes.SNIPED |
Modifier and Type | Method and Description |
---|---|
StiffenerSystemBuilder.EndCutTypes |
SubSystemBuilder.endCutEnd()
Returns the end cut to use at the end of the stiffener sub system.
|
StiffenerSystemBuilder.EndCutTypes |
StiffenerSystemBuilder.endCutEnd()
Returns the end cut to use at the end of the complete stiffener system.
|
StiffenerSystemBuilder.EndCutTypes |
EditStockBuilder.endCutEnd()
Returns the end cut to use at the end of the stiffener sub system.
|
StiffenerSystemBuilder.EndCutTypes |
SubSystemBuilder.endCutStart()
Returns the end cut to use at the start of the stiffener sub system.
|
StiffenerSystemBuilder.EndCutTypes |
StiffenerSystemBuilder.endCutStart()
Returns the end cut to use at the start of the complete stiffener system.
|
StiffenerSystemBuilder.EndCutTypes |
EditStockBuilder.endCutStart()
Returns the end cut to use at the start of the stiffener sub system.
|
static StiffenerSystemBuilder.EndCutTypes |
StiffenerSystemBuilder.EndCutTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerSystemBuilder.EndCutTypes |
StiffenerSystemBuilder.EndCutTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerSystemBuilder.EndCutTypes[] |
StiffenerSystemBuilder.EndCutTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubSystemBuilder.setEndCutEnd(StiffenerSystemBuilder.EndCutTypes endCutEnd)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
StiffenerSystemBuilder.setEndCutEnd(StiffenerSystemBuilder.EndCutTypes endCutEnd)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
EditStockBuilder.setEndCutEnd(StiffenerSystemBuilder.EndCutTypes endCutEnd)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
SubSystemBuilder.setEndCutStart(StiffenerSystemBuilder.EndCutTypes endCutStart)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
StiffenerSystemBuilder.setEndCutStart(StiffenerSystemBuilder.EndCutTypes endCutStart)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
EditStockBuilder.setEndCutStart(StiffenerSystemBuilder.EndCutTypes endCutStart)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.