Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static StiffenerBuilder.AttachmentOption |
StiffenerBuilder.AttachmentOption.INFERRED
Infer the plate on which to attach the stiffener
|
static StiffenerBuilder.AttachmentOption |
StiffenerBuilder.AttachmentOption.OVERRIDE
Use the selected attachment plate on which to attach the stiffener
|
Modifier and Type | Method and Description |
---|---|
StiffenerBuilder.AttachmentOption |
StiffenerBuilder.attachmentPlateOption()
Returns the attachment plate option
License requirements: None. |
static StiffenerBuilder.AttachmentOption |
StiffenerBuilder.AttachmentOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerBuilder.AttachmentOption |
StiffenerBuilder.AttachmentOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerBuilder.AttachmentOption[] |
StiffenerBuilder.AttachmentOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StiffenerBuilder.setAttachmentPlateOption(StiffenerBuilder.AttachmentOption attachmentPlateOption)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.