Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
ShipNamesBuilder |
ShipNamesBuilderList.findItem(int index)
Returns the object at the input index.
|
ShipNamesBuilder[] |
ShipNamesBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
ShipNamesBuilder[] |
ShipNamesListBuilder.setObjectTypes(NXObject[] objects)
Sets the current list of
ShipNamesBuilder objects
to the types determined by the types of the supplied objects. |
ShipNamesBuilder |
StiffenerSystemBuilder.shipNames()
Returns the Ship Names builder, used to assign names to the Stiffener Systems created.
|
ShipNamesBuilder |
StandardPartFrameworkBuilder.shipNames()
Returns the Ship Names builder, used to assign names to the Standard Parts created.
|
ShipNamesBuilder |
SeamBuilder.shipNames()
Returns the Ship Names builder, used to assign names to the Seams created.
|
ShipNamesBuilder |
PlateSystemBuilder.shipNames()
Returns the Ship Names builder, used to assign names to the Plate Systems created.
|
ShipNamesBuilder |
PillarSystemBuilder.shipNames()
Returns the Ship Names builder, used to assign names to the Pillar Systems created.
|
ShipNamesBuilder |
EdgeReinforcementBuilder.shipNames()
Returns the Ship Names builder, used to assign names to the Edge Reinforcement Systems created.
|
Modifier and Type | Method and Description |
---|---|
void |
ShipNamesBuilderList.append(ShipNamesBuilder object)
Appends an object to the list
License requirements: None. |
void |
ShipNamesBuilderList.append(ShipNamesBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ShipNamesBuilderList.erase(ShipNamesBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ShipNamesBuilderList.erase(ShipNamesBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ShipNamesBuilderList.findIndex(ShipNamesBuilder obj)
Finds the index where the input object appears.
|
void |
ShipNamesBuilderList.insert(int location,
ShipNamesBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ShipNamesBuilderList.setContents(ShipNamesBuilder[] objects)
Sets the contents of the entire list.
|
void |
ShipNamesBuilderList.swap(ShipNamesBuilder object1,
ShipNamesBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.