Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ShipCutoutBuilder.CreationMethod |
ShipCutoutBuilder.CreationMethod.FACE2LINES
1 face and 2 lines, edges, or datums are used to place this cutout
|
static ShipCutoutBuilder.CreationMethod |
ShipCutoutBuilder.CreationMethod.SPECIFY_CSYS
a csys is used to place this cutout
|
Modifier and Type | Method and Description |
---|---|
ShipCutoutBuilder.CreationMethod |
ShipCutoutBuilder.placementType()
Returns the placement type.
|
static ShipCutoutBuilder.CreationMethod |
ShipCutoutBuilder.CreationMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShipCutoutBuilder.CreationMethod |
ShipCutoutBuilder.CreationMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShipCutoutBuilder.CreationMethod[] |
ShipCutoutBuilder.CreationMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShipCutoutBuilder.setPlacementType(ShipCutoutBuilder.CreationMethod placementType)
License requirements: nx_ship_concept ("Ship Concept") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.