Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static SectionDrawingBuilder.ViewsPerSheetOptions |
SectionDrawingBuilder.ViewsPerSheetOptions.FIVE |
static SectionDrawingBuilder.ViewsPerSheetOptions |
SectionDrawingBuilder.ViewsPerSheetOptions.FOUR |
static SectionDrawingBuilder.ViewsPerSheetOptions |
SectionDrawingBuilder.ViewsPerSheetOptions.ONE |
static SectionDrawingBuilder.ViewsPerSheetOptions |
SectionDrawingBuilder.ViewsPerSheetOptions.SIX |
static SectionDrawingBuilder.ViewsPerSheetOptions |
SectionDrawingBuilder.ViewsPerSheetOptions.THREE |
static SectionDrawingBuilder.ViewsPerSheetOptions |
SectionDrawingBuilder.ViewsPerSheetOptions.TWO |
Modifier and Type | Method and Description |
---|---|
static SectionDrawingBuilder.ViewsPerSheetOptions |
SectionDrawingBuilder.ViewsPerSheetOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionDrawingBuilder.ViewsPerSheetOptions |
SectionDrawingBuilder.ViewsPerSheetOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionDrawingBuilder.ViewsPerSheetOptions[] |
SectionDrawingBuilder.ViewsPerSheetOptions.values()
Returns an array that contains the values for this enum.
|
SectionDrawingBuilder.ViewsPerSheetOptions |
SectionDrawingBuilder.viewsPerSheet()
Returns the views per sheet
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SectionDrawingBuilder.setViewsPerSheet(SectionDrawingBuilder.ViewsPerSheetOptions sctPerDrawing)
License requirements: nx_ship_drafting ("Ship Drafting") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.