Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
ProfileSystemBuilder |
ShipCollection.createProfileSystemBuilder(ProfileSystem profileSystem)
Creates a
ProfileSystemBuilder . |
Modifier and Type | Interface and Description |
---|---|
interface |
EdgeReinforcementBuilder
Represents a
EdgeReinforcement builder which is used to create or edit a edge reinforcement system feature. |
interface |
PillarSystemBuilder
Represents a
PillarSystem builder which is used to create or edit a pillar system feature. |
interface |
SeamBuilder
A
SeamBuilder used to create or edit a
ship design Seam feature. |
interface |
StiffenerSystemBuilder
This class is used to create or edit a
StiffenerSystem feature. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.