Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PlateChamferBuilder.Types |
PlateChamferBuilder.Types.ON_EDGE
Create a chamfer on the edge
|
static PlateChamferBuilder.Types |
PlateChamferBuilder.Types.TO_PLATE
Create a chamfer on the common edges between plates
|
Modifier and Type | Method and Description |
---|---|
PlateChamferBuilder.Types |
PlateChamferBuilder.type()
Returns the type
License requirements: None. |
static PlateChamferBuilder.Types |
PlateChamferBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateChamferBuilder.Types |
PlateChamferBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateChamferBuilder.Types[] |
PlateChamferBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlateChamferBuilder.setType(PlateChamferBuilder.Types type)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.