Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PlateChamferBuilder.AngleMethod |
PlateChamferBuilder.AngleMethod.ANGLE
Use the angle for the chamfer parameters
|
static PlateChamferBuilder.AngleMethod |
PlateChamferBuilder.AngleMethod.RATIO
Use the ratio for the chamfer parameters
|
Modifier and Type | Method and Description |
---|---|
PlateChamferBuilder.AngleMethod |
PlateChamferBuilder.angleOption()
Returns the angle option
License requirements: None. |
static PlateChamferBuilder.AngleMethod |
PlateChamferBuilder.AngleMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateChamferBuilder.AngleMethod |
PlateChamferBuilder.AngleMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateChamferBuilder.AngleMethod[] |
PlateChamferBuilder.AngleMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlateChamferBuilder.setAngleOption(PlateChamferBuilder.AngleMethod angleOption)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.