Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PlateBuilder.Types |
PlateBuilder.Types.ADOPT
Adopts plate body.
|
static PlateBuilder.Types |
PlateBuilder.Types.CREATE
Creates plate body.
|
Modifier and Type | Method and Description |
---|---|
PlateBuilder.Types |
PlateBuilder.type()
Returns the plate type, which is creation or adoption.
|
static PlateBuilder.Types |
PlateBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateBuilder.Types |
PlateBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateBuilder.Types[] |
PlateBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlateBuilder.setType(PlateBuilder.Types type)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.