Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PlateBuilder.RegionOptions |
PlateBuilder.RegionOptions.ALL |
static PlateBuilder.RegionOptions |
PlateBuilder.RegionOptions.INSIDE_BODY |
static PlateBuilder.RegionOptions |
PlateBuilder.RegionOptions.OUTSIDE_BODY |
Modifier and Type | Method and Description |
---|---|
PlateBuilder.RegionOptions |
PlateBuilder.regionOption()
Returns the region option, which defines the plate areas in case of body faces as plate boundary.
|
static PlateBuilder.RegionOptions |
PlateBuilder.RegionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateBuilder.RegionOptions |
PlateBuilder.RegionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateBuilder.RegionOptions[] |
PlateBuilder.RegionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlateBuilder.setRegionOption(PlateBuilder.RegionOptions regionOption)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.