Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PillarBuilder.EndTypeOptions |
PillarBuilder.EndTypeOptions.CAP
Each end has different end cuts
|
static PillarBuilder.EndTypeOptions |
PillarBuilder.EndTypeOptions.ENDCUT
The same end cut is applied to both ends
|
static PillarBuilder.EndTypeOptions |
PillarBuilder.EndTypeOptions.NONE
No end cuts are applied
|
Modifier and Type | Method and Description |
---|---|
PillarBuilder.EndTypeOptions |
PillarBuilder.endTypeOption()
Returns the end type Option
License requirements: None. |
static PillarBuilder.EndTypeOptions |
PillarBuilder.EndTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PillarBuilder.EndTypeOptions |
PillarBuilder.EndTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PillarBuilder.EndTypeOptions[] |
PillarBuilder.EndTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PillarBuilder.setEndTypeOption(PillarBuilder.EndTypeOptions endTypeOption)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.