Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static DisplaySolidBuilder.DisplayOptionTypes |
DisplaySolidBuilder.DisplayOptionTypes.CURVE |
static DisplaySolidBuilder.DisplayOptionTypes |
DisplaySolidBuilder.DisplayOptionTypes.CURVE_AND_SOLID |
Modifier and Type | Method and Description |
---|---|
DisplaySolidBuilder.DisplayOptionTypes |
DisplaySolidBuilder.displayOption()
Returns the setting for how the basic design objects are displayed.
|
static DisplaySolidBuilder.DisplayOptionTypes |
DisplaySolidBuilder.DisplayOptionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DisplaySolidBuilder.DisplayOptionTypes |
DisplaySolidBuilder.DisplayOptionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DisplaySolidBuilder.DisplayOptionTypes[] |
DisplaySolidBuilder.DisplayOptionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DisplaySolidBuilder.setDisplayOption(DisplaySolidBuilder.DisplayOptionTypes displayOption)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.