Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static DeckBuilder.Types |
DeckBuilder.Types.PLANES
Mold face is being defined by selected or defined planes.
|
static DeckBuilder.Types |
DeckBuilder.Types.ROUND_CAMBER
Mold face is being defined by a generated round camber shape.
|
static DeckBuilder.Types |
DeckBuilder.Types.SHEET_BODY
Mold face is being defined by a selected sheet body.
|
static DeckBuilder.Types |
DeckBuilder.Types.STRAIGHT_CAMBER
Mold face is being defined by a generated straight camber shape.
|
Modifier and Type | Method and Description |
---|---|
DeckBuilder.Types |
DeckBuilder.type()
Returns the method used to define the mold face of the deck.
|
static DeckBuilder.Types |
DeckBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DeckBuilder.Types |
DeckBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DeckBuilder.Types[] |
DeckBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DeckBuilder.setType(DeckBuilder.Types type)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.