Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static SolidPunchBuilder.Types |
SolidPunchBuilder.Types.DIE_TYPE |
static SolidPunchBuilder.Types |
SolidPunchBuilder.Types.PUNCH_TYPE |
Modifier and Type | Method and Description |
---|---|
SolidPunchBuilder.Types |
SolidPunchBuilder.type()
Returns the type
License requirements: None. |
static SolidPunchBuilder.Types |
SolidPunchBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SolidPunchBuilder.Types |
SolidPunchBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SolidPunchBuilder.Types[] |
SolidPunchBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SolidPunchBuilder.setType(SolidPunchBuilder.Types type)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR sheet_metal_design ("SHEET METAL DESIGN") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.