Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
SheetmetalBendState |
SheetmetalBendParameters.bendState
Bend Face is flat or bent
|
SheetmetalBendState[] |
SheetmetalManager.InnerBendFacesData.bendstates
Bend Face is flat or bent
|
static SheetmetalBendState |
SheetmetalBendState.BENT |
static SheetmetalBendState |
SheetmetalBendState.FLAT |
static SheetmetalBendState |
SheetmetalBendState.UNKNOWN |
Modifier and Type | Method and Description |
---|---|
static SheetmetalBendState |
SheetmetalBendState.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SheetmetalBendState |
SheetmetalBendState.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SheetmetalBendState[] |
SheetmetalBendState.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
SheetmetalBendParameters(double innerRadiusInitial,
double neutralFactorInitial,
double bendAngleInitial,
SheetmetalBendState bendStateInitial)
Constructor for the SheetmetalBendParameters object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.