Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Method and Description |
---|---|
SMBoundaryConditionBuilder |
MetaformBuilder.createSMBoundaryCondition()
Create a new boundary condition.
|
SMBoundaryConditionBuilder |
SMBoundaryConditionBuilderList.findItem(int index)
Returns the object at the input index.
|
SMBoundaryConditionBuilder[] |
SMBoundaryConditionBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SMBoundaryConditionBuilderList.append(SMBoundaryConditionBuilder object)
Appends an object to the list
License requirements: None. |
void |
SMBoundaryConditionBuilderList.append(SMBoundaryConditionBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SMBoundaryConditionBuilderList.erase(SMBoundaryConditionBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SMBoundaryConditionBuilderList.erase(SMBoundaryConditionBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SMBoundaryConditionBuilderList.findIndex(SMBoundaryConditionBuilder obj)
Finds the index where the input object appears.
|
void |
SMBoundaryConditionBuilderList.insert(int location,
SMBoundaryConditionBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SMBoundaryConditionBuilderList.setContents(SMBoundaryConditionBuilder[] objects)
Sets the contents of the entire list.
|
void |
SMBoundaryConditionBuilderList.swap(SMBoundaryConditionBuilder object1,
SMBoundaryConditionBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.