Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static LouverBuilder.DepthSideOptions |
LouverBuilder.DepthSideOptions.SECTION_NORMAL_SIDE
Material added on the side of the section normal.
|
static LouverBuilder.DepthSideOptions |
LouverBuilder.DepthSideOptions.SECTION_REVERSE_NORMAL_SIDE
Material added on the side opposite to that of the section normal.
|
Modifier and Type | Method and Description |
---|---|
LouverBuilder.DepthSideOptions |
LouverBuilder.depthSide()
Returns the depth side for the louver.
|
static LouverBuilder.DepthSideOptions |
LouverBuilder.DepthSideOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LouverBuilder.DepthSideOptions |
LouverBuilder.DepthSideOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LouverBuilder.DepthSideOptions[] |
LouverBuilder.DepthSideOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LouverBuilder.setDepthSide(LouverBuilder.DepthSideOptions depthSide)
Sets the depth side for the louver.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.