Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static JogBuilder.FixedSideOptions |
JogBuilder.FixedSideOptions.SECTION_SIDE_LEFT
Side pointed to by the inverse of the tangent cross normal vector
|
static JogBuilder.FixedSideOptions |
JogBuilder.FixedSideOptions.SECTION_SIDE_RIGHT
Side pointed to by the tangent cross normal vector
|
Modifier and Type | Method and Description |
---|---|
JogBuilder.FixedSideOptions |
JogBuilder.fixedSide()
Returns
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static JogBuilder.FixedSideOptions |
JogBuilder.FixedSideOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JogBuilder.FixedSideOptions |
JogBuilder.FixedSideOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JogBuilder.FixedSideOptions[] |
JogBuilder.FixedSideOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
JogBuilder.setFixedSide(JogBuilder.FixedSideOptions sectionSide)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.