Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static JogBuilder.DirectionTypeOptions |
JogBuilder.DirectionTypeOptions.SECTION_NORMAL_SIDE
jog created on the side of the section normal.
|
static JogBuilder.DirectionTypeOptions |
JogBuilder.DirectionTypeOptions.SECTION_REVERSE_NORMAL_SIDE
jog created on the side opposite to that of the section normal
|
Modifier and Type | Method and Description |
---|---|
JogBuilder.DirectionTypeOptions |
JogBuilder.directionType()
Returns
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static JogBuilder.DirectionTypeOptions |
JogBuilder.DirectionTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JogBuilder.DirectionTypeOptions |
JogBuilder.DirectionTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JogBuilder.DirectionTypeOptions[] |
JogBuilder.DirectionTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
JogBuilder.setDirectionType(JogBuilder.DirectionTypeOptions directionType)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.