Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static HemFlangeBuilder.InsetTypeOptions |
HemFlangeBuilder.InsetTypeOptions.BEND_OUTSIDE
The bend and hem flange are outside the thickness face
|
static HemFlangeBuilder.InsetTypeOptions |
HemFlangeBuilder.InsetTypeOptions.MATERIAL_INSIDE
The hem flange is flush with the thickness face on the inside
|
static HemFlangeBuilder.InsetTypeOptions |
HemFlangeBuilder.InsetTypeOptions.MATERIAL_OUTSIDE
The hem flange is flush with the thickness face on the outside
|
Modifier and Type | Method and Description |
---|---|
HemFlangeBuilder.InsetTypeOptions |
HemFlangeBuilder.insetType()
Returns the inset type options
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
static HemFlangeBuilder.InsetTypeOptions |
HemFlangeBuilder.InsetTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HemFlangeBuilder.InsetTypeOptions |
HemFlangeBuilder.InsetTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HemFlangeBuilder.InsetTypeOptions[] |
HemFlangeBuilder.InsetTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HemFlangeBuilder.setInsetType(HemFlangeBuilder.InsetTypeOptions insetType)
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.