Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static GussetBuilder.WidthSides |
GussetBuilder.WidthSides.SIDE1
The Gusset will be created on the side of plane normal of the user defined profile.
|
static GussetBuilder.WidthSides |
GussetBuilder.WidthSides.SIDE2
The Gusset will be created on the opposite side of the plane normal of the user defined profile.
|
static GussetBuilder.WidthSides |
GussetBuilder.WidthSides.SYMMETRIC
The Gusset will be created on both sides of the plane of the user defined profile.
|
Modifier and Type | Method and Description |
---|---|
static GussetBuilder.WidthSides |
GussetBuilder.WidthSides.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GussetBuilder.WidthSides |
GussetBuilder.WidthSides.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GussetBuilder.WidthSides[] |
GussetBuilder.WidthSides.values()
Returns an array that contains the values for this enum.
|
GussetBuilder.WidthSides |
GussetBuilder.widthSide()
Returns the width side
Defines the side of the profile to which material should be added or from which material should be removed to construct the feature. |
Modifier and Type | Method and Description |
---|---|
void |
GussetBuilder.setWidthSide(GussetBuilder.WidthSides widthSide)
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.