Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static GussetBuilder.Shapes |
GussetBuilder.Shapes.ROUND
Specifies a round shape for the Gusset
|
static GussetBuilder.Shapes |
GussetBuilder.Shapes.SQUARE
Specifies a square shape for the Gusset
|
Modifier and Type | Method and Description |
---|---|
GussetBuilder.Shapes |
GussetBuilder.shape()
Returns the shape
See GussetBuilder.Shapes for details. |
static GussetBuilder.Shapes |
GussetBuilder.Shapes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GussetBuilder.Shapes |
GussetBuilder.Shapes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GussetBuilder.Shapes[] |
GussetBuilder.Shapes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GussetBuilder.setShape(GussetBuilder.Shapes shape)
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.