Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions |
FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions.LEFT_DIRECTION
Path adjustment angle left direction.
|
static FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions |
FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions.RIGHT_DIRECTION
Path adjustment angle right direction.
|
Modifier and Type | Method and Description |
---|---|
FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions |
FlexibleCableSegment.pathAdjustmentAngleDirection()
Returns the path adjustment angle direction.
|
static FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions |
FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions |
FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions[] |
FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
FlexibleCableSegment |
FlexibleCableBuilder.createBendSegment(String bendAngle,
String bendRadius,
String pathAdjustmentAngle,
FlexibleCableBuilder.BendAngleDirectionOptions bendAngleDirection,
FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions pathAdjustmentAngleDirection,
int segmentIndex)
Creates a new
Features.SheetMetal.FlexibleCableSegment bend segment. |
void |
FlexibleCableSegment.setPathAdjustmentAngleDirection(FlexibleCableBuilder.PathAdjustmentAngleDirectionOptions pathAdjustmentAngleDirectionOption)
Sets the path adjustment angle direction.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.