Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static FlangeBuilder.MatchFaceOptions |
FlangeBuilder.MatchFaceOptions.NONE
The flange is placed on the selected edge
|
static FlangeBuilder.MatchFaceOptions |
FlangeBuilder.MatchFaceOptions.UNTIL_SELECTED
The flange face is extended until the selected plane
|
Modifier and Type | Method and Description |
---|---|
FlangeBuilder.MatchFaceOptions |
FlangeBuilder.matchFaceOption()
Returns the match face selection type.
|
static FlangeBuilder.MatchFaceOptions |
FlangeBuilder.MatchFaceOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeBuilder.MatchFaceOptions |
FlangeBuilder.MatchFaceOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeBuilder.MatchFaceOptions[] |
FlangeBuilder.MatchFaceOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlangeBuilder.setMatchFaceOption(FlangeBuilder.MatchFaceOptions matchFaceOption)
Sets the match face selection type.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.