Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static FlangeBuilder.LengthTypeOptions |
FlangeBuilder.LengthTypeOptions.INSIDE_DIMENSION
The flange length is dimensioned to the Inner Mold line.
|
static FlangeBuilder.LengthTypeOptions |
FlangeBuilder.LengthTypeOptions.OUTSIDE_DIMENSION
The flange length is dimensioned to the Outer Mold Line.
|
static FlangeBuilder.LengthTypeOptions |
FlangeBuilder.LengthTypeOptions.WEB_DIMENSION
The flange length is dimensioned to the Bend Tangent Line.
|
Modifier and Type | Method and Description |
---|---|
FlangeBuilder.LengthTypeOptions |
FlangeBuilder.lengthType()
Returns a enum indicating the length type.
|
static FlangeBuilder.LengthTypeOptions |
FlangeBuilder.LengthTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeBuilder.LengthTypeOptions |
FlangeBuilder.LengthTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeBuilder.LengthTypeOptions[] |
FlangeBuilder.LengthTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlangeBuilder.setLengthType(FlangeBuilder.LengthTypeOptions lengthType)
Sets a enum indicating the length type.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.