Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static FlangeBuilder.InsetTypeOptions |
FlangeBuilder.InsetTypeOptions.BEND_OUTSIDE
The bend and flange are outside the thickness face
|
static FlangeBuilder.InsetTypeOptions |
FlangeBuilder.InsetTypeOptions.MATERIAL_INSIDE
The flange is flush with the thickness face on the inside
|
static FlangeBuilder.InsetTypeOptions |
FlangeBuilder.InsetTypeOptions.MATERIAL_OUTSIDE
The flange is flush with the thickness face on the outside
|
Modifier and Type | Method and Description |
---|---|
FlangeBuilder.InsetTypeOptions |
FlangeBuilder.insetType()
Returns the inset type (inside, outside, bendoutside) for the flange.
|
static FlangeBuilder.InsetTypeOptions |
FlangeBuilder.InsetTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlangeBuilder.InsetTypeOptions |
FlangeBuilder.InsetTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlangeBuilder.InsetTypeOptions[] |
FlangeBuilder.InsetTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlangeBuilder.setInsetType(FlangeBuilder.InsetTypeOptions insetType)
Sets the inset type (inside, outside, bendoutside) for the flange.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.