Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static ExportFlatPatternBuilder.FileType |
ExportFlatPatternBuilder.FileType.DXF
DXF Export
|
static ExportFlatPatternBuilder.FileType |
ExportFlatPatternBuilder.FileType.TRUMPF_GEO
Trumpf Geo Export
|
Modifier and Type | Method and Description |
---|---|
ExportFlatPatternBuilder.FileType |
ExportFlatPatternBuilder.type()
Returns the type for the flat pattern export.The options are in
ExportFlatPatternBuilder.type() . |
static ExportFlatPatternBuilder.FileType |
ExportFlatPatternBuilder.FileType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExportFlatPatternBuilder.FileType |
ExportFlatPatternBuilder.FileType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExportFlatPatternBuilder.FileType[] |
ExportFlatPatternBuilder.FileType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExportFlatPatternBuilder.setType(ExportFlatPatternBuilder.FileType type)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.