Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static EditCornerBuilder.CornerReliefTypeOptions |
EditCornerBuilder.CornerReliefTypeOptions.CIRCULAR_CUTOUT |
static EditCornerBuilder.CornerReliefTypeOptions |
EditCornerBuilder.CornerReliefTypeOptions.NONE |
Modifier and Type | Method and Description |
---|---|
EditCornerBuilder.CornerReliefTypeOptions |
EditCornerBuilder.cornerReliefType()
Returns the corner relief type
License requirements: None. |
static EditCornerBuilder.CornerReliefTypeOptions |
EditCornerBuilder.CornerReliefTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EditCornerBuilder.CornerReliefTypeOptions |
EditCornerBuilder.CornerReliefTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EditCornerBuilder.CornerReliefTypeOptions[] |
EditCornerBuilder.CornerReliefTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EditCornerBuilder.setCornerReliefType(EditCornerBuilder.CornerReliefTypeOptions cornerRelief)
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.