Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static DimpleBuilder.DepthTypeOptions |
DimpleBuilder.DepthTypeOptions.SECTION_NORMAL_SIDE
Dimple punched on the side of the section normal.
|
static DimpleBuilder.DepthTypeOptions |
DimpleBuilder.DepthTypeOptions.SECTION_REVERSE_NORMAL_SIDE
Dimple punched on the side opposite to that of the section normal
|
Modifier and Type | Method and Description |
---|---|
DimpleBuilder.DepthTypeOptions |
DimpleBuilder.depthType()
Returns the Direction in which the Dimple is punched.
|
static DimpleBuilder.DepthTypeOptions |
DimpleBuilder.DepthTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DimpleBuilder.DepthTypeOptions |
DimpleBuilder.DepthTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DimpleBuilder.DepthTypeOptions[] |
DimpleBuilder.DepthTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DimpleBuilder.setDepthType(DimpleBuilder.DepthTypeOptions depthType)
Sets the Direction in which the Dimple is punched.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.