Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static CornerTreatmentBuilder.CornerTreatmentType |
CornerTreatmentBuilder.CornerTreatmentType.CHAMFER |
static CornerTreatmentBuilder.CornerTreatmentType |
CornerTreatmentBuilder.CornerTreatmentType.NONE |
static CornerTreatmentBuilder.CornerTreatmentType |
CornerTreatmentBuilder.CornerTreatmentType.RADIUS |
Modifier and Type | Method and Description |
---|---|
CornerTreatmentBuilder.CornerTreatmentType |
CornerTreatmentBuilder.treatmentType()
Returns the treatment type option menu value
License requirements: None. |
static CornerTreatmentBuilder.CornerTreatmentType |
CornerTreatmentBuilder.CornerTreatmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CornerTreatmentBuilder.CornerTreatmentType |
CornerTreatmentBuilder.CornerTreatmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CornerTreatmentBuilder.CornerTreatmentType[] |
CornerTreatmentBuilder.CornerTreatmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CornerTreatmentBuilder.setTreatmentType(CornerTreatmentBuilder.CornerTreatmentType treatmentType)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.