Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static ContourFlangeBuilder.SweepSideOptions |
ContourFlangeBuilder.SweepSideOptions.SECTION_NORMAL_SIDE |
static ContourFlangeBuilder.SweepSideOptions |
ContourFlangeBuilder.SweepSideOptions.SECTION_REVERSE_NORMAL_SIDE |
Modifier and Type | Method and Description |
---|---|
ContourFlangeBuilder.SweepSideOptions |
ContourFlangeBuilder.sweepSide()
Returns the projection direction of contour flange
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static ContourFlangeBuilder.SweepSideOptions |
ContourFlangeBuilder.SweepSideOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ContourFlangeBuilder.SweepSideOptions |
ContourFlangeBuilder.SweepSideOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ContourFlangeBuilder.SweepSideOptions[] |
ContourFlangeBuilder.SweepSideOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ContourFlangeBuilder.setSweepSide(ContourFlangeBuilder.SweepSideOptions sweepSide)
Sets the projection direction of contour flange
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.