Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeTransitionBuilder.WidthOptions |
BridgeTransitionBuilder.WidthOptions.FINITE
Bridge Transition starts at specified point on start edge and extends on one side by the specified distance.
|
static BridgeTransitionBuilder.WidthOptions |
BridgeTransitionBuilder.WidthOptions.FULL_BOTH_EDGES
Bridge Transition spans the full length of both the edges.
|
static BridgeTransitionBuilder.WidthOptions |
BridgeTransitionBuilder.WidthOptions.FULL_END_EDGE
Bridge Transition spans the full length of end edge.
|
static BridgeTransitionBuilder.WidthOptions |
BridgeTransitionBuilder.WidthOptions.FULL_START_EDGE
Bridge Transition spans the full length of start edge.
|
static BridgeTransitionBuilder.WidthOptions |
BridgeTransitionBuilder.WidthOptions.SYMMETRIC
Bridge Transition starts at specified point on start edge and extends on either side by half the specified distance.
|
Modifier and Type | Method and Description |
---|---|
static BridgeTransitionBuilder.WidthOptions |
BridgeTransitionBuilder.WidthOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeTransitionBuilder.WidthOptions |
BridgeTransitionBuilder.WidthOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeTransitionBuilder.WidthOptions[] |
BridgeTransitionBuilder.WidthOptions.values()
Returns an array that contains the values for this enum.
|
BridgeTransitionBuilder.WidthOptions |
BridgeTransitionBuilder.widthType()
Returns the width type
License requirements: nx_flexible_pcb ("NX Flexible PCB") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Modifier and Type | Method and Description |
---|---|
void |
BridgeTransitionBuilder.setWidthType(BridgeTransitionBuilder.WidthOptions widthType)
License requirements: nx_flexible_pcb ("NX Flexible PCB") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.