Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeTransitionBuilder.TypeOptions |
BridgeTransitionBuilder.TypeOptions.FOLD
Bridge Transition type consisting of Planar-Bend-Planar regions.
|
static BridgeTransitionBuilder.TypeOptions |
BridgeTransitionBuilder.TypeOptions.ZU
Bridge Transition type consisting of Bend-Planar-Bend regions.
|
Modifier and Type | Method and Description |
---|---|
BridgeTransitionBuilder.TypeOptions |
BridgeTransitionBuilder.type()
Returns the transition type
License requirements: nx_flexible_pcb ("NX Flexible PCB") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
static BridgeTransitionBuilder.TypeOptions |
BridgeTransitionBuilder.TypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeTransitionBuilder.TypeOptions |
BridgeTransitionBuilder.TypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeTransitionBuilder.TypeOptions[] |
BridgeTransitionBuilder.TypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeTransitionBuilder.setType(BridgeTransitionBuilder.TypeOptions type)
License requirements: nx_flexible_pcb ("NX Flexible PCB") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.