Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeTransitionBuilder.InsetOptions |
BridgeTransitionBuilder.InsetOptions.MATERIAL_INSIDE
Bridge Transition body near tangential plane and start will be on same side of the tangential plane selected.
|
static BridgeTransitionBuilder.InsetOptions |
BridgeTransitionBuilder.InsetOptions.MATERIAL_OUTSIDE
Bridge Transition body near tangential plane and start will be on opposite sides of the tangential plane selected.
|
Modifier and Type | Method and Description |
---|---|
BridgeTransitionBuilder.InsetOptions |
BridgeTransitionBuilder.insetType()
Returns the inset type
License requirements: nx_flexible_pcb ("NX Flexible PCB") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
static BridgeTransitionBuilder.InsetOptions |
BridgeTransitionBuilder.InsetOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeTransitionBuilder.InsetOptions |
BridgeTransitionBuilder.InsetOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeTransitionBuilder.InsetOptions[] |
BridgeTransitionBuilder.InsetOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeTransitionBuilder.setInsetType(BridgeTransitionBuilder.InsetOptions insetType)
License requirements: nx_flexible_pcb ("NX Flexible PCB") OR adv_sheet_metal_dsgn ("ADVANCED SHEET METAL DESIGN") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.