Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BreakCornerBuilder.TypeOptions |
BreakCornerBuilder.TypeOptions.CHAMFER_EQUAL_SETBACK |
static BreakCornerBuilder.TypeOptions |
BreakCornerBuilder.TypeOptions.FILLET |
Modifier and Type | Method and Description |
---|---|
BreakCornerBuilder.TypeOptions |
BreakCornerBuilder.type()
Returns the type of the break corner.
|
static BreakCornerBuilder.TypeOptions |
BreakCornerBuilder.TypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BreakCornerBuilder.TypeOptions |
BreakCornerBuilder.TypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BreakCornerBuilder.TypeOptions[] |
BreakCornerBuilder.TypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BreakCornerBuilder.setType(BreakCornerBuilder.TypeOptions type)
Sets the type of the break corner.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.