Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BendTaperBuilder.BendTaperSides |
BendTaperBuilder.BendTaperSides.BOTH
Both Sides
|
static BendTaperBuilder.BendTaperSides |
BendTaperBuilder.BendTaperSides.SIDE1
Side 1 only
|
static BendTaperBuilder.BendTaperSides |
BendTaperBuilder.BendTaperSides.SIDE2
Side 2 only
|
static BendTaperBuilder.BendTaperSides |
BendTaperBuilder.BendTaperSides.SYMMETRIC
Symmetric.
|
Modifier and Type | Method and Description |
---|---|
BendTaperBuilder.BendTaperSides |
BendTaperBuilder.taperSides()
Returns the taper sides
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static BendTaperBuilder.BendTaperSides |
BendTaperBuilder.BendTaperSides.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendTaperBuilder.BendTaperSides |
BendTaperBuilder.BendTaperSides.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendTaperBuilder.BendTaperSides[] |
BendTaperBuilder.BendTaperSides.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BendTaperBuilder.setTaperSides(BendTaperBuilder.BendTaperSides taperSides)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.