Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BendTaperBuilder.BendTaperInputMethod |
BendTaperBuilder.BendTaperInputMethod.ANGLE
Angle
|
static BendTaperBuilder.BendTaperInputMethod |
BendTaperBuilder.BendTaperInputMethod.DISTANCE
Distance
|
static BendTaperBuilder.BendTaperInputMethod |
BendTaperBuilder.BendTaperInputMethod.TO_END
To End
|
Modifier and Type | Method and Description |
---|---|
BendTaperBuilder.BendTaperInputMethod |
BendTaperBuilder.bendTaperInputMethod1()
Returns the input method for side 1
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
BendTaperBuilder.BendTaperInputMethod |
BendTaperBuilder.bendTaperInputMethod2()
Returns the input method for side 2
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static BendTaperBuilder.BendTaperInputMethod |
BendTaperBuilder.BendTaperInputMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendTaperBuilder.BendTaperInputMethod |
BendTaperBuilder.BendTaperInputMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendTaperBuilder.BendTaperInputMethod[] |
BendTaperBuilder.BendTaperInputMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BendTaperBuilder.setBendTaperInputMethod1(BendTaperBuilder.BendTaperInputMethod bendTaperInputMethod1)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
void |
BendTaperBuilder.setBendTaperInputMethod2(BendTaperBuilder.BendTaperInputMethod bendTaperInputMethod2)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.