Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BendBuilder.BendDirectionOptions |
BendBuilder.BendDirectionOptions.SECTION_NORMAL_SIDE
Bend is created on the side of the section normal.
|
static BendBuilder.BendDirectionOptions |
BendBuilder.BendDirectionOptions.SECTION_REVERSE_NORMAL_SIDE
Bend is created on the side opposite to that of the section normal
|
Modifier and Type | Method and Description |
---|---|
BendBuilder.BendDirectionOptions |
BendBuilder.direction()
Returns the Bend Direction
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static BendBuilder.BendDirectionOptions |
BendBuilder.BendDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendBuilder.BendDirectionOptions |
BendBuilder.BendDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendBuilder.BendDirectionOptions[] |
BendBuilder.BendDirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BendBuilder.setDirection(BendBuilder.BendDirectionOptions direction)
Sets the Bend Direction
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.