public static class AeroJoggleBuilder.SideType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SIDE1
Side 1 (only side of single)
|
static int |
_SIDE2
Side 2
|
static AeroJoggleBuilder.SideType |
SIDE1
Side 1 (only side of single)
|
static AeroJoggleBuilder.SideType |
SIDE2
Side 2
|
Modifier and Type | Method and Description |
---|---|
static AeroJoggleBuilder.SideType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AeroJoggleBuilder.SideType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AeroJoggleBuilder.SideType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AeroJoggleBuilder.SideType SIDE1
public static final AeroJoggleBuilder.SideType SIDE2
public static final int _SIDE1
public static final int _SIDE2
public static AeroJoggleBuilder.SideType valueOf(int value)
public static AeroJoggleBuilder.SideType valueOf(String name)
public static AeroJoggleBuilder.SideType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.