Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static RasterImage.MaxTextureSize |
RasterImage.MaxTextureSize.N1024
1024 x 1024 max size
|
static RasterImage.MaxTextureSize |
RasterImage.MaxTextureSize.N16384
16384 x 16384 max size
|
static RasterImage.MaxTextureSize |
RasterImage.MaxTextureSize.N2048
2048 x 2048 max size
|
static RasterImage.MaxTextureSize |
RasterImage.MaxTextureSize.N32768
32768 x 32768 max size
|
static RasterImage.MaxTextureSize |
RasterImage.MaxTextureSize.N4096
4096 x 4096 max size
|
static RasterImage.MaxTextureSize |
RasterImage.MaxTextureSize.N512
512 x 512 max size
|
static RasterImage.MaxTextureSize |
RasterImage.MaxTextureSize.N8192
8192 x 8192 max size
|
Modifier and Type | Method and Description |
---|---|
RasterImage.MaxTextureSize |
RasterImage.maximumTextureSize()
Returns the enum value for the maximum size of the image, in pixels
License requirements: None. |
static RasterImage.MaxTextureSize |
RasterImage.MaxTextureSize.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RasterImage.MaxTextureSize |
RasterImage.MaxTextureSize.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RasterImage.MaxTextureSize[] |
RasterImage.MaxTextureSize.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
RasterImage |
FeatureCollection.createRasterImage(Point3d origin,
Matrix3x3 matrix,
double length,
double height,
String imageFileName,
double translucency,
RasterImage.MaxTextureSize maximumTextureSize)
Creates a raster image
License requirements: studio_visualize ("STUDIO VISUALIZE") . |
void |
RasterImage.update(Point3d origin,
Matrix3x3 matrix,
double length,
double height,
String imageFileName,
double translucency,
RasterImage.MaxTextureSize maximumTextureSize)
Updates a raster image feature
License requirements: studio_visualize ("STUDIO VISUALIZE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.