Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FitCurveBuilder.FittingParametersOptions |
FitCurveBuilder.FittingParametersOptions.DEGREE_AND_SEGMENTS
Fit to degree and segments
|
static FitCurveBuilder.FittingParametersOptions |
FitCurveBuilder.FittingParametersOptions.DEGREE_AND_TOLERANCE
Fit to degree and tolerance
|
static FitCurveBuilder.FittingParametersOptions |
FitCurveBuilder.FittingParametersOptions.TEMPLATE_CURVE
Fit to template spline
|
Modifier and Type | Method and Description |
---|---|
FitCurveBuilder.FittingParametersOptions |
FitCurveBuilder.fittingParameters()
Returns the fitting parameters
License requirements: None. |
static FitCurveBuilder.FittingParametersOptions |
FitCurveBuilder.FittingParametersOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FitCurveBuilder.FittingParametersOptions |
FitCurveBuilder.FittingParametersOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FitCurveBuilder.FittingParametersOptions[] |
FitCurveBuilder.FittingParametersOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FitCurveBuilder.setFittingParameters(FitCurveBuilder.FittingParametersOptions fittingParameters)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.