public static class FitCurveBuilder.FittingParametersOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEGREE_AND_SEGMENTS
Fit to degree and segments
|
static int |
_DEGREE_AND_TOLERANCE
Fit to degree and tolerance
|
static int |
_TEMPLATE_CURVE
Fit to template spline
|
static FitCurveBuilder.FittingParametersOptions |
DEGREE_AND_SEGMENTS
Fit to degree and segments
|
static FitCurveBuilder.FittingParametersOptions |
DEGREE_AND_TOLERANCE
Fit to degree and tolerance
|
static FitCurveBuilder.FittingParametersOptions |
TEMPLATE_CURVE
Fit to template spline
|
Modifier and Type | Method and Description |
---|---|
static FitCurveBuilder.FittingParametersOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FitCurveBuilder.FittingParametersOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FitCurveBuilder.FittingParametersOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final FitCurveBuilder.FittingParametersOptions DEGREE_AND_SEGMENTS
public static final FitCurveBuilder.FittingParametersOptions DEGREE_AND_TOLERANCE
public static final FitCurveBuilder.FittingParametersOptions TEMPLATE_CURVE
public static final int _DEGREE_AND_SEGMENTS
public static final int _DEGREE_AND_TOLERANCE
public static final int _TEMPLATE_CURVE
public static FitCurveBuilder.FittingParametersOptions valueOf(int value)
public static FitCurveBuilder.FittingParametersOptions valueOf(String name)
public static FitCurveBuilder.FittingParametersOptions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.