public static class SectionSurfaceBuilder.ControlRegionEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_END
depth and skew applied to the end section of the section surface
|
static int |
_ENTIRE
depth and skew applied to the entire section surface
|
static int |
_START
depth and skew applied to the start section of the section surface
|
static SectionSurfaceBuilder.ControlRegionEnum |
END
depth and skew applied to the end section of the section surface
|
static SectionSurfaceBuilder.ControlRegionEnum |
ENTIRE
depth and skew applied to the entire section surface
|
static SectionSurfaceBuilder.ControlRegionEnum |
START
depth and skew applied to the start section of the section surface
|
Modifier and Type | Method and Description |
---|---|
static SectionSurfaceBuilder.ControlRegionEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilder.ControlRegionEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilder.ControlRegionEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final SectionSurfaceBuilder.ControlRegionEnum ENTIRE
public static final SectionSurfaceBuilder.ControlRegionEnum START
public static final SectionSurfaceBuilder.ControlRegionEnum END
public static final int _ENTIRE
public static final int _START
public static final int _END
public static SectionSurfaceBuilder.ControlRegionEnum valueOf(int value)
public static SectionSurfaceBuilder.ControlRegionEnum valueOf(String name)
public static SectionSurfaceBuilder.ControlRegionEnum[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.