Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilder.ControlRegionEnum |
SectionSurfaceBuilder.ControlRegionEnum.END
depth and skew applied to the end section of the section surface
|
static SectionSurfaceBuilder.ControlRegionEnum |
SectionSurfaceBuilder.ControlRegionEnum.ENTIRE
depth and skew applied to the entire section surface
|
static SectionSurfaceBuilder.ControlRegionEnum |
SectionSurfaceBuilder.ControlRegionEnum.START
depth and skew applied to the start section of the section surface
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilder.ControlRegionEnum |
SectionSurfaceBuilder.controlRegion()
Deprecated.
Deprecated in NX9.0.0. Use
SectionSurfaceBuilderEx instead.
|
static SectionSurfaceBuilder.ControlRegionEnum |
SectionSurfaceBuilder.ControlRegionEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilder.ControlRegionEnum |
SectionSurfaceBuilder.ControlRegionEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilder.ControlRegionEnum[] |
SectionSurfaceBuilder.ControlRegionEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilder.setControlRegion(SectionSurfaceBuilder.ControlRegionEnum controlRegion)
Deprecated.
Deprecated in NX9.0.0. Use
SectionSurfaceBuilderEx instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.